Part Number: LM741
I have encountered multiple failures of the LM741CH operational amplifier ICs. In operation, these ICs are configured for a voltage follower configuration as part of a most negative input voltage auctioneering circuit. The failures observed were not hard failures in that they were still providing an output however, the output did not correspond to the input voltage and was out of tolerance for the voltage follower configuration. I was wondering what failure mode for this op amp was possible in order to produce an output that did not equal the input when set up for a follower configuration. I know they do have offset null pins that could impact the output, however, these pins are not used or connected when in use in this application. Both diodes were checked to be functioning properly. Thank you.