Part Number: INA826
Other Parts Discussed in Thread: INA286,
Hi Everyone,
I am using INA826 for current measurement. Input SHUNT_A and SHUNT_B is connected to 100R resistor for current 0-10 mA.
I have problem because when current circuit is open (current is equal to 0 mA) a have output offset 21 mA on INA826.
INA286 is powered -5V to (-26) V.
When i use for simulations TINA software this problem doesn't exist, everything will work ok.
All devices is connect to the same GND.