Part Number: THS4302
Other Parts Discussed in Thread: LMH6703, OPA855, OPA858, THS4304
Hi,
I am looking for an amplifier with similar specs to the THS4302 to use as a DAC buffer (or potentially selecting the THS4302 itself).
We are needing an amplifier capable of 1Vpp (50 Ohm matched load, so 2Vpp at amplifier output), and 0.5Vpp 1-2GHz. The THS4302 seems like a good choice with a high bandwidth and very high slew rate.
When I am looking at interfacing with our DAC (current sourcing complementary outputs), the inbuilt feedback resistors of the THS4302 might make it hard for us to design a well matched differential to single ended conversion stage with the THS4302. Specifically achieving good CMMR, which depends on the matching of the input resistors.
Are there any examples of using the THS4302 as a DAC buffer, or any other TI amplifiers that would be recommended for this application?
Thanks
Jordan