Part Number: TLV1701
Could you pls help to calculate how much higher the VIN- voltage is than the VIN+ voltage, the output voltage jumps? Thanks

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Fabio,
I'm assuming the "VDD33" is 3.3V.
The output should "jump" as soon as the two input voltages cross, typically within a millivolt or two.
The R10/R11 dividers set up a reference voltage of 1.10V at the positive input.
The voltage at pin 3 needs to go below 1.100 for the output to go high, and above 1.100 to go output low.
The TLV1701 has a maximum internal offset voltage of ±5.5mV.
Ideally, the threshold is 1.1V, but you should take into account the worst case input offset voltage.
To make the input go high, Pin 3 (neg input) needs to be less than 1.1V - 5.5mV = 1.0945V
To make the input go low, Pin 3 (neg input) needs to be less than 1.1V + 5.5mV = 1.1055V.
The VBUS_OUT divider ratio is 21.04 - so the VBUS_OUT thresholds will be 21.04 times the above threshold voltages.