Hello Team,
We are using LM13700 in our design for audio limiter application, we have not used the second operational amplifier. Can we leave the second Op-Amp pins Floating?
As shown in below screenshot can we leave the highlighted pins floating.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Team,
We are using LM13700 in our design for audio limiter application, we have not used the second operational amplifier. Can we leave the second Op-Amp pins Floating?
As shown in below screenshot can we leave the highlighted pins floating.
Hey Pavan,
Please see the following E2E post on how to configure your unused amplifier. Terminating Pin 16 to V- will ensure no bias current. The rest can be left floating.
Best,
Jerry
Unused outputs can (and should) be left open.
In general, unused op-amp inputs should be properly biased. But see figure 16:
In theory, if you leave the inputs (pins 1,2,3,4,7) open, no current will flow. But they might pick up noise, so it would be safer to connect them to V−.
Thank you both for quick reply,
So, to summarize we can leave the output pin as floating (12,9), remaining inputs (10,13,14,15,16) should be grounded, such it can be prevented from noise pick on other amplifier.
What about Diode bias input(2,15) can we it as floating, does this pin also have effect on noise pickup.
Hey Pavan,
Diode bias is just a connection to the inputs through a diode, so it could still pick up noise but it will have ~0.7V less noise pickup than the input pins.
Best,
Jerry
Pavan,
The first reply is an acceptable solution. There are many other good solutions. The only 'bad' solutions are shorting outputs, connecting inputs out of normal range, and have open pins connected to long traces (antenna).