Part Number: LM393
Hello developers
Are there any regulations for the rise of the input waveform and the rise time?
Does the output oscillate if the rise/fall time is slow?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM393
Hello developers
Are there any regulations for the rise of the input waveform and the rise time?
Does the output oscillate if the rise/fall time is slow?
There is no specified limit, but if the input is too slow, the output might indeed oscillate (because the switching noise or other noise might shift the voltage at the input).
All comparators used with slow signals should have hysteresis. Some devices have built-in hysteresis; with the LM393, you would need to add positive feedback. See, for example, Comparator with and without hysteresis circuit.