This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

VFC110: VFC110AP use of 2016 and Older

Part Number: VFC110


Hello

In my last post I had mentioned that I was falling short of some 200 Nos

of  VFC110 / VFC110AP / VFC110AP-2 for a Project of ours.

I have procured the rest from Rochester and some Distributors.

I have been offered some with a Date Code of 2010 & 2016.

My question is whether I can use 7 year or 12 year old IC's VFC110

or their two variants.

Besides Non compliance to ROHS , can there be any other issues 

regarding their functionality and/or the variation due to aging of the

Internal Cos ( Approx 50 pF ) ?

Varun

  • Hi Varun,

    Yes I remember your challenges, I wish there was more we could to do help get you more devices.

    Regarding device shelf lifetimes, generally this comes down to moisture sensitivity.  A device that has been sitting on the shelf in a humid environment may start to absorb moisture, and the package/die interface will be degraded.  When this occurs, there can be detrimental effects to the performance of the device.  I can't say for sure if the capacitor itself would be impacted but the mechanism behind capacitor failures on, say, film or electrolytic capacitors, would be different than a capacitor on a silicon die. 

    However if the product has been stored properly and maintained the proper packaging, then it should be OK; see the following website for more details:

    https://www.ti.com/support-quality/faqs/product-shelf-life-faqs.html

    Please review the info. above and let us know if there's anything we can help clarify.

    Regards,
    Mike

  • Hi Mike

    Thanks a lot for your reply.

    I shall ask the source if the storage was as per the recommendations 

    and I am indeed glad that you mention : "If stored properly should be okay even after 7 Yrs 

    Heartfelt thanks for your answers & support to me in the past

    on many occasions.

    Thanks again & have a great day ahead 

    Varun