Other Parts Discussed in Thread: INA129
Hi,
in chapter 6.5 of the DS of the INA129-EP, what is "Overtemperature" test conditions ?
Characteristics (Offset voltage, CMR, Bias &n Offset currents, Gain error, Nonlinearity, etc) are given both at nominal test condition & "overtemperature" test condition (ex for G&in error: test cond1: G=1, test.cond2 = overtemperature). There are 2 columns referring to the same TA=25°C with different performance. I am struggling with this overtemperature test condition which is not envolved for instance in the INA129UA DS...
In our design we would like to change the uspcreened part (-55°C/+125°C) of INA129UA with the extended mil range of the INA129-EP whose features are very similar. Are the two references with the same die ? with the INA-129EP upscreened by TI ?
Many thanks,
Pascal