Other Parts Discussed in Thread: XTR108
Hello,
I'm still working in a project that uses the XTR108 as a temperature transmitter. We design the circuit to work with it, but isn't work. When I turn on the voltage source, there are no voltage signal through the resistors Rz1...Rz5. I don't know why it is happening. When that happens, we can't measure any voltage signal through the Pt100 too, so we can't measure the temperature variation. If I remove the resistors (Rz1 to Rz5), I can measure voltage in those terminals.
I've checked all the circuit diagram, and it is equal to a version that alreary worked as expected. The system that program the SPI EEPROM is working correctly, so I would like to know if someone already seen something similar to help me. What can be happening?
Thanks in advance.
Juliana