Part Number: OPA810
When I set up this sim with the 2020 model, I get 2.1Mhz F-3dB not the reported 3Mhz. That number is pretty close to equation 10 using an extracted GBP of 66MHz. 2.1MHz is also closer to Table 9.2 -was this a mistake or am I missing something? Also, 100kohm is a 100dB DC gain, not 90dB,