Other Parts Discussed in Thread: OPA333, TINA-TI, INA333, OPA340, INA332
Hi, I an using a tina-TI version 9 and trying to do a simulation on a circuit using the INA333 and OPA333. I downloaded the the spice models form the TI site. I am trying to create a portion of a ECG circuit that is shown in the data sheet for the INA333, figure 37. When I set up my first simulation using the ina333 and opa333 separately, things behaved as expected. This was with separate voltage sources on each input. The DC analysis works fine, with both balanced inputs and when I introduced a DC differential on the inputs, the difference times the gain gave me the expected output. INA333 gain was 10m opa333 gain was 100
Then I connected the output of the INA333 to the input of the opa333, hoping for a total gain of 1000. When I perfrom the DC analysis, I get an error message:operating point not found, U1,D17. I am using the default TINA-TI parameters.
For a simple circuit like this, I thought the sumulation should be straightforward. Am I overlooking something simple?
Dan
The INA333 output is connected