This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC34RF52IRTD_Carrier Material Report

Hi  TI Team,

ADC34RF52IRTD Carrier Material Report  is not available on TI.com. 

I could not confirm the description in the data sheet.

Could you provide the materials?

Material name : ADC34RF52IRTD 

Best regards,


Sakamoto

TOKYO ELECTRON DEVICE LIMITED (TED)

 

  • Hi Sakamoto,

    We don't have this available yet so I am checking on this for you. Kindly await a response. Thank you for your patience.

    Regards, Chase

  • Thank you for contacting me. Please continue to provide materials as they become available.

    Regards,

  • Hi Misuzu,

    Please find details about this tray below. Instead of qty 168, note the actual value is 260.

    Descriptor          : for QFN 9 x 9 MM                                       
    Supplier            : Daewon                                                 
    Supplier Number     : 14L-0909-B19                                           
    Tray Matrix         : 26 x 10                                                
    Material            : PES                                                    
    Standard            : JEDEC                                                  
    Temperature Max     : 150   DEG C

    Regards, Chase