This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL084H: In/Out limitation

Part Number: TL084H
Other Parts Discussed in Thread: TLV9001, TLV9051

Hi team,

When customer try the below non-inverting circuit, customer see non-linear in V_IN<0.3V. Vcc=5V, Vee=GND

If I understand correctly, Vcm should be 1.5V < Vcm < 5V from datasheet. Also Vcm = V_IN. I'm not sure why there is linear in <1.5V.

Also output voltage swing limitation is also violated since its head room exists.

What is the solution for this case? lets change opamp to rail-to-rail or Vee should be negative supplied, right?

Best regards,

Hayashi