Part Number: LM2901
Hi team,
can the LM2901 (either B or non B version) withstand -1V from Vcc to GND (not to the input pins).
Datasheet seems to not give an absolute minimum, only the maximum voltage here.
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM2901
Hi team,
can the LM2901 (either B or non B version) withstand -1V from Vcc to GND (not to the input pins).
Datasheet seems to not give an absolute minimum, only the maximum voltage here.
Thanks!
Hello Stephanie,
The Abs Max says -0.3V for the LM2901B.
It should be similar for the LM2901. Both are on similar processes.
Neither one will like it..
These are junction isolated processes, so the body diode (substrate) will be in full conduction. Damage can occur if the current is not limited.