Part Number: LM10
I have a similar question about the reference pins. I am using the LM10CN/NOPB as a unity gain buffer amplifier between a high-impedance output sensor and our scope and lab DA system, which have an identical input impedance to our sensor. This has worked very well until recently and now we are seeing some weird stuff with the system and I'm wondering if there may be some problems with the buffer amp circuit. I am only using the op amp with inputs on pins and 2&3 and output on 6. Vcc on 7 is 1.8V and pin 4, V- is at ground.
I've not connected any of the other pins to anything. Should I? Will Reference Output and Reference Feedback affect op amp "#1"?
Thanks!
WC