Other Parts Discussed in Thread: LM2901, TLV1805-Q1, TLV1704-Q1, , LM339
Hi Experts:
It set VCC of LM2901 is 9~16V, IN+ =VCC/2 :
When IN- is equal to VCC-0.7V,is the out`pin output high?
When IN- is equal to 0V,is the out`pin output low?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Experts:
It set VCC of LM2901 is 9~16V, IN+ =VCC/2 :
When IN- is equal to VCC-0.7V,is the out`pin output high?
When IN- is equal to 0V,is the out`pin output low?
No; it's the opposite. The output is high when the non-inverting input IN+ is higher than the inverting input IN−. In other words, the output follows the signal at IN+, or inverts the signal at IN−.
Please note that VCC − 0.7 V is outside the valid input voltage range. The LM2901B-Q1 can still work when only one input has an invalid voltage, but the electrical characteristics (especially propagation delay) are no longer guaranteed. Better use a comparator with rail-to-rail inputs like the TLV1704-Q1 or TLV1805-Q1.
Hello Zhang,
Please see sections 2.5, 2.7 and 2.8 of the LM339 family application note:
Application Design Guidelines for LM339, LM393, TL331 Family Comparators
As Clemens mentioned, you would be relying on an expected result, but not guaranteed. TI will always recommend staying within the recommended input specifications (Vcc-2V).
Hi Paul:
We haved viewed the documents,we corrected the designing as below:
1、VCC=9V,when 1IN-=3V, 1IN+=5.6V ,Output is High; when 1IN-=3V, 1IN+=0.1V output islow.
2、VCC=16V, when 1IN-=5.2V, 1IN+=10V ,Output is High;1IN-=3V, 1IN+=0.1V output is low.
Can we get the result what we want? Please help us to review it

Yes; the circuit will work with these values.
In the image, the GND pin and the inputs of the unused comparators are floating. I guess this will not be the case in the real circuit.