This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV2262AM: TLV2262AMJGB The actual product does not match the model

Part Number: TLV2262AM

Hi

According to the datasheet, the two packages represent different models. The correct package of our model should be: JG (all feet are the same width), but the real thing is a "P" package (two feet are narrow), TLV2262AMJGB, according to the datasheet is CDIP 8Pin, now the actual PDIP 8Pin and datasheet does not match
pin PIN is also inconsistent with the datasheet. Please confirm whether the package of this product is changed or whether the real product is inconsistent with TLV2262AMJGB