Part Number: TLV521
Dears,
Just curious what's the purpose for adding a transistor in the sensing circuit? Generally, without the transistor, just use an op-amps could monitor the current.

Hugh
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TLV521
Dears,
Just curious what's the purpose for adding a transistor in the sensing circuit? Generally, without the transistor, just use an op-amps could monitor the current.

Hugh
Hello Hugh,
The V+ voltage is 'noise' which is an unwanted signal that should be eliminated or tolerated. If V+ much larger than Vsense then the 'noise' is much bigger than the signal, 'Vsense' ; therefore very accurate resistors would be needed for a regular difference amplifier setup (to get high CMRR).
For figure 36, the voltage is converted to a current then back into a voltage referenced to ground. The errors are Q1 base current, so consider Darlington PNP or PMOS transistor. and Vout must not be loaded (needs high impedance destination)
In all cases the opamp's input voltage offset error is an error source.