I bought four TAS5424CQ1DKEEVM evaluation boards and I connected all of them to the same PC using their USB-to-I2C boards.
I use the TAS54x4C EVM GUI, SLOC287, to control the amplifiers.
However, I can only see one of them at each time, and not control all of them.
Is there a way to connect all of them to a PC and controlling them simultaneously using the TAS54x4C EVM GUI?
Thanks!!