Other Parts Discussed in Thread: ISO224, , AMC1350
Dear Experts, Can I use this part for measuring AC signals of up to a 10KHz, since its bandwidth is typically 300KHz.
Regards,
Rajesh BN.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Rajesh,
Yes, 10kHz is fine.
What type of application is the measurement for?
The application is inverter control. I am planning to measure the current from a hall sensor. The fundamental current of the hall sensor is 400Hz and it has harmonics upto 15KHz. The hall sensor converts the current signal to instantaneous voltage signal varies between +/-4V. These signals are processed and connects to a microcontroller board. I want the microcontroller's ground to be isolated from the mentioned signal. Furthermore ,the voltage signal is a single ended bipolar signal.
Does the AMC1351 works with bipolar signal? Would you suggest any IC that's in ur mind? I had an IC in my mind- ISO224. Issue with this is, the I/p voltage range of this IC is +/-12V, and the signal of my interest is +/-4V. AMC1351 perfectly suits my application which is 5V. But, in the data sheet it's nowhere mentioned -5V.
Regards,
Rajesh BN.
Hi Rajesh,
Thank you for the background. Apologies my previous post was incorrect, I was focused on the bandwidth question. The correct device to consider is the AMC1350. This device has a +/-5V input voltage range.