There is a schematic diagram in which the +vs =24V ,-VS=Ref=0v, +IN < 24v , +IN > -IN >0v and G=1 as following: 
Question: Is the equation true ?
Vout = G*(IN+ - IN- )
Thanks,
John
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
John,
Connecting IN+ to positive rail violates the maximum input common-mode voltage defined to be from (V-) to (V+)-1V - see below. Thus, the circuit will NOT work.


Keep in mind that the linear input voltage range of INA826 is a function not only of supply voltage, gain and Vref but also of Vcm as shown below.