Part Number: LMH6552
Hi team,
Could you help check the schematic as below? Inout AC=1.5V Vpp, DC=0V, power supply is ±5V, but the output voltage follows the positive voltage. For example, when the power supply is 5V, the output voltage is above 4V not attend to 5V, and when the power supply is 4V, the output voltage is above 3V not attend to 4V. And they tried to adjust the gain=1, and the output still follows the power supply.