Other Parts Discussed in Thread: INA851
Hello,
I am designing a circuit in which a differential input signal is amplified with the INA851 and the PGA855 and then digitized with the ADS981X A/D converter. The amplifiers are supplied with +-15V, the DIffernet input signal is maximum +-13V. The smallest one is 4.7mV. The question is how I have to interconnect the three devices with respect to the pins VOCM and FDA. Can I set VOCM of the INA851 and PGA855 to ground? And how high do I choose the capacitors between the output and FDA?
Thanks a lot