This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA4354-Q1: OPA4354-Q1

Part Number: OPA4354-Q1
Other Parts Discussed in Thread: OPA4354

Hi TI team,

I am using OPA4354 IC to provide PWM to Mos-fet in step down converter. application is automotive. I usually preferred Schmitt trigger + integration + comparator/error type for my design to reduce other components and it should be closed loop to control my output voltage, so output feedback preferred.

My design parameter's are

1. Required Switching frequency - 650Khz/1.5uS

2. Duty cycle-  37%

3. Step down input & output voltage - 12V(input) & 5V(output)

4. Feedback voltage - 1V to 2.5V (can adjust as per requirement)

 I am confused, how to provide 1st pulse to start circuit and to get feedback voltage for control/set output voltage.

I request you to kindly provide simulation model, component calculation with basic op-amp with simulation result to get clarity about other component calculation

Thanks in advance