Hello,
unfortuantely the original case has been locked already "TLV9164: SO# 944207 - Per customer the parts are not solderable..."
The customer now mentioned:
-----
" You are referring to the wrong readings.
The illustration with the red and blue lines only shows the process window resulting from the components used.
Under point 8 (8 Prozessdaten - TOP) you will find the actual measurement
results measured on the printed circuit board.
As you can see, the heating and cooling gradients (Max+ 3K/s and Max -6K/s) are not violated.
TL to TP = 2,8 K/s
TP to TL = -5,1 K/s
------
Can you still advise on this?
Thank you