This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM7372: OrCAD Capture PSpice Model

Part Number: LM7372
Other Parts Discussed in Thread: TINA-TI

Can TI provide an OrCAD Capture PSpice .DSN with a working LM7372 part? Thank you. 

  • Hello Ryan,

    Please utilize the .mod model file in the existing LM7372 PSPICE model zip folder.  You can find this under "Design & Development" on the LM7372 product page.

    You may then open or import this model into PSPICE.  One way to do this is to start a new PSPICE project & design in Capture; you should be able to start with a blank schematic.  You then navigate to the portion of PSPICE where you browse for parts to ''place."  You will find a button to add a library to the design; using this button you can pull the LM7372 model into your schematic design, and add the necessary resistors & capacitors for your simulation.

    While TI does provide TINA-TI Reference Design circuits alongside models for some ICs, the only modelling file available for the LM7372 is the .mod file and the explanation .txt file.  There is not a TINA-TI Reference Design file or a similar basic simulation design with the LM7372 in its default configuration.

    You will have to import the model and build up your own schematic around the op-amp.

    Best,

    Alec