Part Number: INA350
Hi everyone,
I have a problem with INA350CDS. I'm trying to read the temperature from a PT1000, connected to a Wheatstone bridge. I powerised the instrumental amplifier at 3V3, but the output resultan gets saturated around 0,6V no matter the gain selected. If the input x gain=50 is less that 0,6V the amplification works properly, but once this Vin x G overpasses 0,6V, the output gets stucked and you can see no difference between G =30 and G=50.
The configuration I used is very close to this from the datasheet.

I used a protoboard to test the circuit, I don't know if bad connections might be introducing some noise that might be interfering with a proper performance. I just want to know if anybody have faced a similar problem or if there might be a problem with the configuration. As far as I understand this AI fits perfectly for this kind of applications isn't it?
Xavier