Part Number: PGA309EVM-USB
Other Parts Discussed in Thread: PGA309,
Good morning,
i'm trying to use the PGA309EVM-USB with USB DAQ Platform and PGA309 Test board.
Making use of the USB_DAQ + PGA309EWM.ppt. i created a configuration file, disabling the sensore emulation.
I connected a load cell, with a 350 ohm bridge and sensitivity of 2mV/V, to the PGA test board, and using the PGA309 Calculatore software, i found Coarse offset, Front end PGA Zero DAC, GAIN DAC and ouput amp gain.
I enabled Internal Vref, to 2.5V, and Sensore excitation to 1.3V and VSA to 5V.
The PGA309 Test board configuration is in Vout 4 wire and the jumper settings are the following:
JMP4 ext
JMP5 ext
JMP13 DIODE
JMP6 ext
JMP7 nc
JMP8 one to prg
JMP3 ADS1
JMP9 nc
JMP1 nc
JMP17 ext
JMP 12 Vexc
JMP11 vdut
JMP10 nc
If i measure Vref and Vsensor (usign a multimeter), i read 2.5 V and 1.28V, parameters that i set but i don't see Vout variation when apply a known weight on the cell.
Problably i'm doing something wrong, any suggestions?
Thanks in advance,
Carmelo