Dear e2e team,
I need to supply the TLV9351IDBVR with V+=+3.3V and V-=-5V: looking at the datasheet, at pag 7 table 6.1 there is Vsupply= V+ - V- = 0-42V, instead at table 6.3 is (V+) – (V–) = 4.5 V to 40 V (±2.25 V to ±20 V).
So +3.3V is lower than the given 4.5V but it s still compatible for the range with dual supply (±2.25 V to ±20 V).
Is there any limitations by using the TLV9351IDBVR in these conditions?
Thanks,
Giorgia