Part Number: XTR115
Other Parts Discussed in Thread: XTR111
Dear Sirs,
Is there a very simple way to limit the maximum current the XTR115 can emit - rather than letting it saturate at the 32mA range?
Anywhere between 23 and 26 mA would be fine for what i need.
The input voltage will vary between 11 - 30V.
The external transistor used is FZT853.
The load resistance is upto 500 Ohm.
Thanks
Carl