Other Parts Discussed in Thread: TINA-TI
I trying to simulate a circuit that amplifies a differential input, that comes from a inductor with two coils, and the comom wire is connected to reference voltage of 0.8VDC.
The circuit is equal to the one in the picture below. We have a dua coil Inductor, with a reference voltage of 0.8VDC, the coils of the inductor will be stimulated by a magnetic field. The capture signal at the output of the inductor is 1mV, over the 0.8VDC.

As I don’t know how to simulate it as it is, I used the circuit below, but I saw in one post the usage of VCVS to dp something similar.

VG4 and VG3 respectively.

Both with DC level equals to 0.
There is way to simulate the circuit closely to the real usage, with the dual inductor?