This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC1100: Output phase shift at low frequencies

Part Number: AMC1100


Hi, i'm using an AMC1100 upstream of an ADC for sensing and need accurate gain and output phase values for it to account for them in the ADC. In Tina i've simulated the spice model and it gives me around -0.06 degrees phase shift at 50hz, is that accurate? If it isn't where can i find the correct values?

Many thanks

  • Hi Robin,

    Using a 3 us delay and a 20 ms period I got a 0.054 degree phase shift. So, I believe your -0.06 degree phase shift sounds reasonable. Note, it is subject to change based on maximum specification for signal delay though. Please let me know if you have any more questions.

    Best regards,

    Eva