Part Number: LMH6401EVM
Other Parts Discussed in Thread: LMH6401, OPA855DSGEVM, OPA855
Hi there,
I was trying to test the LMH6401EVM output with the square wave input.
As shown in the figure below, the green and purple channels are the differential inputs (positive and negative).
The yellow and blue channels are the outputs. It seems that the step response is over-damped.

The DC power input is +-2.4V.
My question is how to obtain the critically-damped response?
Can we change some resistor and capacitor values to realize this? Any model can be used for simulation?
Thanks and best,
Yilun