Part Number: OPA2189
Other Parts Discussed in Thread: OPA189
Hi,
When I use OPA2189,
The values of ELVSS_DAC3 and VGNG_ELVSS remain unchanged,
The ratio of R45, R204, R52 and R53 remains the same, and the maximum output range measured at opamp output pin 1 changes when the resistance value changes (the maximum output value can reach -20V when the resistance value becomes smaller =1.5Kohm, and the maximum output value can reach -18V when the resistance =100Kohm). Please help analyze the reason for this problem:
1. Help check whether +5V and -23V power supply can be used for the op amp?
2, R45, R204, R52, R53 these four resistance values are different will affect the performance of the op amp?

Many thanks~