Part Number: JFE150
I see that the TINA model for the JFE150 now incorporates the nominal parameters as well as the 'strong' and 'weak' editions. How do I tell TINA to use these variations?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: JFE150
I see that the TINA model for the JFE150 now incorporates the nominal parameters as well as the 'strong' and 'weak' editions. How do I tell TINA to use these variations?
Hey Dennis,
Did you download the zip file shown below?

When you download this zip file it will contain the 3 variants:

Best Regards,
Chris Featherstone
Thanks Chris. No, I did not download the entire '.zip' file for the model. I had downloaded the reference design (SLPM351A.TSC) and saw the three options in the macro of the part. My hope was that there was a way to have the tool step through the three model variations as parameters.
Hi Dennis,
I reached out to our modeling expert. The recommendation was to remove and place each TSM as needed. There isn't a way to have the tool step through the three model variations as parameters because process variations can change more than one parameter to do model parameterization.
Best Regards,
Chris Featherstone