Part Number: INA214
Hi Team
For INA214
- What is the lowest minus voltage that IN+\IN- can withstand(based on GND)? it's GND-0.3?
- Is the GND-0.3V stable value or instantaneous value? if it's a instantaneous value, hong long of the time limitation?
- note (3)describes that if the current input into IN+\IN- pin is smaller than 5mA,the voltage on IN+\IN- can exceed the rang from GND-0.3V to 26. what's the minus limitation voltage under this conditions?
- if IN+\IN- was damage because of the voltage is exceed -0.3V. the IN+\IN- will be open or short to PGND ?