This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO122: can iso122 be used to add dc shift to output signal.

Part Number: ISO122


imagine ISO122 has Vs1 as +/-5V and input is -1V, the VS2 is 0-10V , what will be output voltage ?

Should it be 4V, as input is -1V for a input voltage range of -5 to 5v in the same manner the output shall be 4v in the power range of 0 - 10V.