Hello, I was redoing the calculations in the detailed design section to use in my own project. I find the RSNS-EFF value, which is 9.96 kOhm in the photo, to be approximately 50.352 kOhm. I want to ask, am I making a mistake or is there an error in the data sheet?ti /resized-image/__size/320x240/__key/communityserver-discussions-components-files/14/T_3101_forumquestion1.png