Other Parts Discussed in Thread: LMH6611,
Hi TI,
What is difference for LMH34400 and LMH6611 output voltage when enable / disbale Ambient Light Cancellation Mode of LMH34400?
According to LMH34400 data sheet :
7.3.3 Single-Ended Output Stage
The output stage of the LMH34400 has a 10-Ω series resistor on its output to isolate the amplifier output stage
transistors from the package bond-wire inductance and printed circuit board (PCB) capacitance. The net gain of
the LMH34400 (TIA + output stage) is 40 kΩ when driving an external 100-Ω resistor. When the external load
resistor is increased above 100 Ω, the effective gain from the IN pin to the output pin increases. Consequently,
when the external load resistor is decreased to less than 100 Ω, the effective gain from the IN pin to the output
pin decreases as a result of the larger voltage drop across the internal 10-Ω resistor. When there is no load
resistor connected to the output pin, the effective TIA gain is 44 kΩ. The output voltage of the LMH34400 is set
to a fixed value of 1.0 V when there is no current flowing into the amplifier. The output swings above and below
1.0 V when the photodiode sinks and sources current, respectively.
For below schematic, if there is no input ,whether is LMH6611 output voltage expected @3.5V (1V x 3.5 (LMH6611 gain)) ?, but actually to measure LMH6611 output volatge is 3.29V , why?
if input 19.5uW into PD-3 and expected 18.5uA flow into LMH34400, whether is the LMH6611 output DC level @3.5V (1V x 3.5) ? and the LMH6611 output swings above and below 3.5V ?
and is the swing volatge level @ 18.5uA x 40 K x 3.5 = 2.59V which is over the supply volatge @4.5V (+Vop)?
For below schematic, how to connect external 100-Ω resistor for LMH34400's loading ?