Part Number: AMC3330
Hello
I am designing an Iot device powered via isolated power supply from the 230VAC main sector. we need to measure the 230VAC via an isolated measrment systeme
I identified the AMC3330,
my questions are :
I want to measure the input voltage via a 3V3 microcontroller system, the AMC3330 ( using 1,6Meg and 10K resistors as requested in the datasheet is powered via 5VDC) : any recomendation to deliver a single ended Analog signal to the ADC ?
I tryed to use the spice model with Tina and Ltspice, it is not working : any hints about simulation models please ?
best regards
Ziad