Dear team,
Can you please help provide some suggestions on whether the output pin1 of TL074 had such ripple when disconnected V3.3?
Even on IU_AD it has the ripple as well refer to below capture..
The negative terminal of pin 2 is the 2.5V output from the Hall device, and the positive terminal of pin 3 is the 2.5V reference voltage divider input.