Other Parts Discussed in Thread: UCC28950,
Good morning.
I am using the LMC6484 and transistor MMBT2222ALT1 as a current source to sink current and change the voltage feedback on the UCC28950. The input for the + on the LMC6484 comes from a Digital to Analog Converter with a voltage range of 0V to 2V. Depending on the input voltage from the DAC, the feedback voltage will change and will make the output voltage on my converter change to my desired output. Please see a reduced schematic below.
Note: The DAC output is with respect to GND.
I am running into some problems when using the LMC6484 in this application, particularly when the input from the DAC is disconnected or 0V. This circuit shouldn't be doing anything when there is no input from the DAC, but it is causing a lot of jitter on my feedback voltage for the UCC28950. I have cut the trace that connects this part of the circuitry to the UCC28950 and there was no jitter after that, so I know it is related to the circuitry around the LMC6484. Module 1 seems to be almost immune to this jitter effect, probably because it is the module closest to where the LMC6484 circuitry lives and closest to GND. Module 2 is worse than Module 1, and Module 3 is the worst by far. Module 3 is the one furthest away from the circuitry around the LMC6484.
When the DAC is 1V, and the circuitry is sinking current, there is still some noticeable jitter at the feedback of the UCC28950, but not nearly as bad as when the DAC input is disconnected or 0V.
Do you have any recommendations to mitigate this effect?
Thank you for your time.
Alberto Miguez