Part Number: AMC1350
Other Parts Discussed in Thread: AMC1400
Hi, I am wondering why all the Ti's isolated amplifiers have net gain of 2v (i.e. AMC1400 0.25V input, fixed gain of 8V/V =>2V outs/ AMC1350 +/-5V input, fixed gain 0.4v/v=>2) The ADC I am using is the tms320F28397D, with the differential ADC (two ADC channels). Thus, if i use this combination, I will only be using 60% resolution of the ADC (0-3.3.V)?
Thanks
Jack