I want to use two cascaded op amps with a NPN transistor to feed the coil of a relay. Does anyone have any design suggestions? The input voltage is in range of 0 to 20mV and it is not DC. it is harmonic. I mean by harmonic is that it goes to a speaker and create a sound.
Your help is much appreciated.