Part Number: AMC1311EVM
Other Parts Discussed in Thread: AMC1311
Please specify the overall dimensions of the EVM board
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AMC1311EVM
Other Parts Discussed in Thread: AMC1311
Please specify the overall dimensions of the EVM board
Hi Mohammed,
Welcome to our e2e forum! Can I ask why you need the dimensions of the AMC1311EVM?
Hi Tom,
To mount this board in a test rack. Also, I would like to know about the max current consumption at VDD2 input (3.0V to 5.5V DC, Default configuration at VDD1 input 5V).
Please specify maximum current consumption so that we can select a proper power supply. Note that we need to power two AMC13111 EVM board from a single power supply. How much Ampere power supply will be most suitable for this application.
Hi Mohammed,
This test rack, is it for production testing or are you trying to evaluate the AMC1311?