Part Number: ALM2402-Q1
Other Parts Discussed in Thread: ALM2402FQ1EVM
Hello experts,
Hope you are doing well.
Here are some questions when my customer do SCG (short circuit to ground) and SCB (short circuit to battery) test. Kindly invite you to offer some help.
1. SCG
There is an OTF/SH_DN pin in ALM2402-Q1, our customer pull up this pin to 5V through a 10kohm resistor, they did SCG test under different ambient temperature, but found different voltage on the pin:
① When -40℃, the OTF pin 2.52V
② When 25℃, the OTF pin 3.743V
③ When 105 ℃, the OTF pin 3.685V
There are several questions:
- what is the recommended pullup resistor of SH_DN pin;
- what is the internal structure of this pin, why it is affected by temperature?
- It seems that OTF function didn't occur in SCG test under 105C, what's the reason, and then how can MCU find the SCG fault?

2. SCB
When the output short to battery (set 16V by voltage source), the chip was damaged.
Our field team think maybe the supplier voltage rushed to 18V when power on, which is limit of Vcc_(ox), so what is your idea?
And for voltage limit, our customer think 18V is constrained, what is the reason here, and how to improve this situation? (because they think it's usual for the battery voltage exceed the limit)
![]()
Thanks very much. Looking forward to your reply.