Other Parts Discussed in Thread: OPA657
OPA 657 works as an current to voltage converter. It has 30M (30 000 000 ohms) resistor in feedback loop and the problem is that noise mesured on the output (bandwidth is limited to 150kHz by RC filter)is aprox 15mVp-p (!) This seems to be very much to much fro this amp.
In Datasheet we can read that it has 1,6fA /(sqrHz) current input noise. 1,fA by 30 meg of feedback resistor should give 48nV / sqr(Hz) . Let's asume 150KHz BW, it should be 18uV (not 20mV).......
The ampliffier is shileded, it has 10uF 0805 (Tayo Yuden) decoupling and 10R power rails separator.
I did not toook thermal noise into account, because it's vwry low in this case and it's not aplified.
What could be wrong?