Hi team,
Are there internal clamping diode between IN+/- and V-?

Does it need to add the diodes below?

BRs,
Haury
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
Are there internal clamping diode between IN+/- and V-?

Does it need to add the diodes below?

BRs,
Haury
Yes, these internal diodes exist.
External diodes might be helpful to avoid a current through the internal diodes; see section 2.4 of the Application Design Guidelines for LM324 and LM358 Devices.
Hello Haury,
Internal diodes are present. External diodes will share the input current flow. However voltage more negative than -300mV may cause phase reversal.