Hello,
The datasheet is unclear on whether the INA238-Q1 will load the I2C bus when unpowered and when the address pins (A0, A1) are connected to either SDA or SCL. Will they load down the I2C bus? Will they allow back powering through the INA238-Q1?
The datasheet implies no back powering through the SDA and SWCL pins alone, but says nothing about the address pins:
Thank you,
Jeff