This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH6703: 500MHz noise at output when there is no input even after using the recommended RF value

Part Number: LMH6703


Hi,

I am using LM6703MA as a unity gain amplifier and gain=0.8V but I observed a 500MHz oscillation noise with 500mV Vp-p at the output even after I got a 50ohm termination the input. I am using recommended RF = 390ohm. Is the noise expected? If not please advise.

Thanks.

Regards,

Isaac